I am using the LMT84LP temp sensor and I am running into issues where the output voltage will randomly drop from 0.9V to something in the range of 0.2 - 0.6V. It will jump around from a good output voltage to a bad output voltage far a while until the sensor fails with a very low output voltage. The sensor is powered from 3.3V and the filter is 100Ω in series with a 2.2uF cap to ground. The signal then goes into an STM32 processor.
I have a number of sensors connected like this but it is only 1 particular sensor that fails. Has anybody seen anything similar to this?