HELLOW
We have multiple units of the same product, and we are monitoring their amplitudes to be consistent. However, there are significant differences in the fluctuation of distance measurements. What could be the reason for this?
Thank YOU
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HELLOW
We have multiple units of the same product, and we are monitoring their amplitudes to be consistent. However, there are significant differences in the fluctuation of distance measurements. What could be the reason for this?
Thank YOU
Meiling.
Can you define "significant differences in the fluctuation of distance measurements"? What do you mean by this. How different are they in mm? What is the total distance to the target when you have the fluctuations of distance?
Gordon.
At 4m, the distance fluctuation is about ±25mm. At 8m, the distance fluctuation is about ±85mm
Meiling,
At 4m having a +/-25mm fluctuation is less than 1% error. At 8m having a +/-85mm fluctuation is right at 1%. Overall the accuracy is very good. If the fluctuation is causing an issue then increase the averaging in the OPOT3101. typically 32 or 64 is a good averaging value. Increase sample rate to overcome slow averaging response. It looks like you have a good system.
Gordon,
1. I have set the average value and the parameters are set as follows.
2.How to select the parameters of Auto HDR Scale and H Threshold?
Meiling,
Both of these settings are for advanced use. Almost always they should be set to the default settings. I have never seen a user that needed to change these settings.
Super HDR ratio should be 64
H Threshold should be 26000