Other Parts Discussed in Thread: J784S4XEVM, DCA1000EVM, AWR2544, AWR2944, TDA4VP-Q1, TDA4AP-Q1, TDA4AH-Q1, TDA4VH-Q1
We want to setup a centralised/satellite radar system. Where we can have 4 to 5 radars streaming 1DRFFT data to a processor board. The processor board is able to read from 4/5 radars streaming data via 1GBPS Ethernet ports and then execute signal processing algorithms on the 4/5 radars streaming 1D RFFT data in real-time.
So, for the radars streaming 1D RFFT data can we use AWR2544LOP evaluation module with the DCA1000EVM (Also does AWR2544 support DDMA alike AWR2944) and for the processing board to read from 4/5 radars via the 4*1GBPS ports can we use J784S4XEVM. Or do you already have a setup for the satellite radar system?