This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL6432: Failed to run CAN in APP if adding CAN operation in SBL

Part Number: AWRL6432


Hi,

My customer added CAN operation (polling mode) in SBL to TX/RX CAN message but found the CAN can't work ok in APP.

They did a lot of test and found if they added 20s delay after Enable Clock for FECSS, CAN works ok in APP.

I suggested customer to add MCAN_txBufCancellationReq before WDT reset (without 20s delay) in SBL, but still failed.

Would you pls kindly advise what may be missed in SBL for MCAN deinit? 

Thanks,

Chris