Hello,
I have a technical question regarding the PGA900.
I want to use the PGA900 to output calibrated sensor values via UART. While I have confirmed that the PGA900 supports various output options as listed below, I would like to verify if UART output is also possible.
Output options:
- Ratiometric and absolute voltage output
- 4- to 20-mA current loop interface
- One-wire interface (OWI) over power line
- PWM output
- Serial peripheral interface (SPI)
- Inter-integrated circuit (I2C)
Thank you for your assistance.
Best regards,