This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Raw data capture without mmwaveStudio

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR6843AOP

Tool/software:

Hello,

I want to capture raw data from IWR6843AoP EVM (Rev. F) using DCA1000  and/or mwmave EICBoost , without mmwaveStudio.

I wanted to measure in continuous mode ( 1 chirp per frame) and at a higher frame rate  (say 200Hz or more). Kinldy let me know if this is possible.

Also, please let me know what version of mmwave SDK should I use and also which demo firmware to flash.

Thanks and Regards

Vignesh