This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: Unable to display the point cloud.

Part Number: IWR1843BOOST

Tool/software:

IWR1843BOOST can't get point cloud via ti_mmwave_rospkg under ubuntu system when there is no problem with wiring and power supply.

  • Hello,

    Can you confirm that the .launch files you are using is sending the CLI commands to the correct port? On Ubuntu if you do "ll /dev", you should be able to find ttyUSB0 and 1 OR ttyACM0 and 1. Make sure the .launch file has it correctly written, as well as the IWR1843BOOST itself being set to functional mode via switches on the EVM after the correct firmware is flashed in flashing mode.

    Best Regards,

    Pedrhom