Tool/software:
Our company is developing a project called an alcohol chain device, with an estimated annual usage of 700k
We have selected TI's temperature and humidity sensor, model: HDC1080DMBR, DFN-6 (3x3).
Currently encountering the following issues:
HDC1080, after successful communication establishment. Only the device ID number can be read, and the temperature and humidity values cannot be read. It is empty and defaults to zero.
Please help us check what the problem is and provide a solution, thank you!
The following are schematic diagrams and software for reference
#include "dmm_hdc1080.h" #include "dmm_function.h" #include "dmm_gpio.h" #include "dmm_systick.h" #include "dmm_timer_module.h" #include "math.h" //******************************************************************************************// #define IIC_DELAY 50 //******************************************************************************************// static void iic_start(void) { SDA_OUT_H; delay_us(IIC_DELAY); SCL_OUT_H; delay_us(IIC_DELAY); SDA_OUT_L; delay_us(IIC_DELAY); SCL_OUT_L; delay_us(IIC_DELAY); } //******************************************************************************************// static void iic_stop(void) { SCL_OUT_L; delay_us(IIC_DELAY); SDA_OUT_L; delay_us(IIC_DELAY); SCL_OUT_H; delay_us(IIC_DELAY); SDA_OUT_H; delay_us(IIC_DELAY); } //******************************************************************************************// static uint8 iic_wait_ack(void) { uint8 ERROR_TIME=0; SDA_OUT_H; delay_us(IIC_DELAY); SCL_OUT_H; delay_us(IIC_DELAY); while(SDA_IN) { ERROR_TIME++; if(ERROR_TIME>250) {iic_stop();return 1;} } SCL_OUT_L; delay_us(IIC_DELAY); return 0; } //******************************************************************************************// static void iic_ack(void) { SCL_OUT_L; delay_us(IIC_DELAY); SDA_OUT_L; delay_us(IIC_DELAY); SCL_OUT_H; delay_us(IIC_DELAY); SCL_OUT_L; delay_us(IIC_DELAY); } //******************************************************************************************// static void iic_no_ack(void) { SCL_OUT_L; delay_us(IIC_DELAY); SDA_OUT_H; delay_us(IIC_DELAY); SCL_OUT_H; delay_us(IIC_DELAY); SCL_OUT_L; delay_us(IIC_DELAY); } //******************************************************************************************// static void iic_send_byte(uint8 txd) { uint8 t; SCL_OUT_L;delay_us(IIC_DELAY); for(t=0;t<8;t++) { if((txd&0x80)>>7) SDA_OUT_H; else SDA_OUT_L; txd<<=1; delay_us(IIC_DELAY); SCL_OUT_H; delay_us(IIC_DELAY); SCL_OUT_L; delay_us(IIC_DELAY); } } //******************************************************************************************// static uint8 iic_read_byte(uint8 ack) { uint8 i,receive=0; SDA_OUT_H;delay_us(IIC_DELAY); for(i=0;i<8;i++ ) { SCL_OUT_L; delay_us(IIC_DELAY); SCL_OUT_H; delay_us(IIC_DELAY); receive<<=1; if(SDA_IN) receive++; } if(!ack) iic_no_ack(); else iic_ack(); return receive; } //******************************************************************************************// extern void HDC1080_Write_Register(u8 Addr,u16 Data) { unsigned char data[2]; data[0] = (uint8_t)((Data& 0xFF00) >> 8); //¸ß°ËλÊý¾Ý data[1] = (uint8_t)(Data & 0x00FF); //µÍ°ËλÊý¾Ý iic_start(); iic_send_byte(HDC1080_WRITE_ADDR);iic_wait_ack(); //µØÖ·Îª10000000£¬Ð´¼Ä´æÆ÷ iic_send_byte(Addr);iic_wait_ack(); //д¼Ä´æÆ÷µØÖ· iic_send_byte(data[0]);iic_wait_ack(); //·¢Ë͸߰ËλÊý¾Ý iic_send_byte(data[1]);iic_wait_ack(); //·¢Ë͵ͰËλÊý¾Ý iic_stop(); //Í£Ö¹ÐźŠ} //******************************************************************************************// unsigned char HDC1080_Read_Register(unsigned char ReadAddr,unsigned char *buf,unsigned int length) { uint8_t i = 0; iic_start(); //ÆðʼÐźŠiic_send_byte(HDC1080_WRITE_ADDR); //HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R) iic_wait_ack(); //²úÉúÓ¦´ð iic_send_byte(ReadAddr); //¼Ä´æÆ÷µØÖ· iic_wait_ack(); //²úÉúÓ¦´ð iic_start(); //ÆðʼÐźŠiic_send_byte(HDC1080_READ_ADDR); //HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R) ¶Á iic_wait_ack(); //²úÉúÓ¦´ð for(i = 0; i < length-1; i++) { buf[i] = iic_read_byte(1); //¶ÁÊý¾Ý } buf[i] = iic_read_byte(0); //¶ÁÊý¾Ý iic_stop(); //Í£Ö¹ÐźŠreturn 0; } //******************************************************************************************// void Read_TH_Register(unsigned char *pbuff) { uint8_t length = 4, i = 0; //ת»»Êý¾Ý×Ö½ÚÊý iic_start(); //ÆðʼÐźŠiic_send_byte(HDC1080_WRITE_ADDR); //HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R) iic_wait_ack(); //²úÉúÓ¦´ð iic_send_byte(HDC1080_TEMPERATURE_ID); //´¥·¢Ê¼þµØÖ· iic_wait_ack(); //²úÉúÓ¦´ð iic_stop(); delay_ms(50); //µÈ´ýת»¯ iic_start(); //ÆðʼÐźŠiic_send_byte(HDC1080_READ_ADDR); //HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R) ¶Á iic_wait_ack(); //²úÉúÓ¦´ð for(i = 0; i < length-1; i++) { pbuff[i] = iic_read_byte(1); //¶ÁÊý¾Ý } pbuff[i] = iic_read_byte(0); iic_stop(); //Í£Ö¹ÐźŠ} //******************************************************************************************// void HDC1080_Driver_Init(void) { uint8_t menufacture_buf[2] = {0}, device_buf[2] = {0}; uint16_t menufacture_id = 0, device_id = 0; HDC1080_Read_Register(HDC1080_MENUFACTURE_ID, menufacture_buf, 2); menufacture_id = (uint16_t)(menufacture_buf[0]<<8); menufacture_id |= menufacture_buf[1]; HDC1080_Read_Register(HDC1080_DEVICE_ID, device_buf, 2); device_id = (uint16_t)(device_buf[0]<<8); device_id |= device_buf[1]; if(menufacture_id==HDC1080_MENUFACTURE_ID_VALUE&&device_id==HDC1080_DEVICE_ID_VALUE) { printf("<-----HDC1080 Á¬½Ó³É¹¦£¡----->\r\n"); } else printf("<-----HDC1080 Á¬½Óʧ°Ü£¡----->\r\n"); //ÉèÖÃͬʱ²É¼¯Î¶ȺÍʪ¶È 14λ·Ö±æÂÊ Ö»Òª·¢ËÍÒ»¸ö´¥·¢ÃüÁîÎÂʪ¶È¾Í»áÁ¬Ðø×¼»» HDC1080_Write_Register(HDC1080_CONFIG_ID, HDC1080_CONFIG_VALUE); } //******************************************************************************************// void Get_HDC1080_THValue(float *temp, float *humid) { uint8_t buf[4] = {0}; //¶ÁÎÂʪ¶È¼Ä´æÆ÷Öµ±£´æÔÚÊý×éÖÐ Read_TH_Register(buf); //ζÈת»» *temp = (float)(buf[0]<<8|buf[1]); *temp = (*temp/pow(2,16))*165-40; //ʪ¶Èת»» *humid = (float)(buf[2]<<8|buf[3]); *humid = (*humid/pow(2, 16))*100; } //******************************************************************************************// .h #ifndef _DMM_DMM_HDC1080_H_ #define _DMM_DMM_HDC1080_H_ /******************************************************************************/ #include "dmm_type.h" /******************************************************************************/ //¼Ä´æÆ÷µØÖ· typedef enum{ HDC1080_WRITE_ADDR = 0x80, HDC1080_READ_ADDR = 0x81, HDC1080_MENUFACTURE_ID = 0xfe, HDC1080_DEVICE_ID = 0xff, HDC1080_CONFIG_ID = 0x02, HDC1080_TEMPERATURE_ID = 0x00, HDC1080_HUMIDITY_ID = 0x01, }REGISTER_ADDR; //¼Ä´æÆ÷Öµ typedef enum { HDC1080_MENUFACTURE_ID_VALUE = 0x5449, HDC1080_DEVICE_ID_VALUE = 0x1050, HDC1080_CONFIG_VALUE = 0x1000, //ÎÂ¶È Êª¶Èͬʱת»» 14λ·Ö±æÂÊ }REGISTER_VALUE; void HDC1080_Driver_Init(void); extern void HDC1080_Write_Register(u8 Addr,u16 Data); unsigned char HDC1080_Read_Register(unsigned char ReadAddr, unsigned char *buf, unsigned int length); void Read_TH_Register(unsigned char *pbuff); void Get_HDC1080_THValue(float *temp, float *humid); /******************************************************************************/ #endif