Tool/software:
Hello!
I am developing a sensor to detect people using the IWR6843AOP. The demo uses the area scanner, and the configuration is the default cfg from the radar toolbox.
I want to detect a person moving very slowly at about 6 meters, but with the default cfg, no dynamic points are generated (or only very few points appear occasionally).
I have tried changing the cfarcfg for range and doppler to lower the threshold. While I observed a significant increase in dynamic points (including noise due to the increased signal) at closer distances, there was no significant change in dynamic points for a person moving very slowly at around 6 meters (the number of points slightly increased, but the number of valid dynamic points remained the same).
Besides changing the cfarcfg threshold, are there any other solutions I could try (such as increasing the Rxgain in profilecfg)?
Or is it inherently difficult to detect a person moving very slowly at a distance of 6 meters with the IWR6843AOP?
Please let me know if there are any more effective methods.
Thank you.