Tool/software:
Hi TI team,
I am processing LDC1614 multi-channel measurement. I want to measure the time delay of two coils (two channels). When I try setting sampling interval from 80ms to 10ms, the resolution decreases. That is, sampling interval at 10ms, I can't tell the target waveform from the Noise. There are two question I'm going to ask you. First, how low could i set up my sampling interval to measure(perhaps the main reason is ADC)? Second, if the previous difficulty can't be solved, which board would meet my needs(sampling interval could be set at least 5ms with high resolution)?
Thanks,
En-Zhu, Lyu