This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: AWR1443 and ESP32 SPI Communication

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1443

Tool/software:

Hello all,

I am working with the AWR1443BOOST board, and I'm wanting to pass the raw data from the AWR to an XIAO-ESP32C3 via SPI. I turned the S1 switch to the SPI position and have connected what I think are the correct SPI pins. Here are the connections that I have so far:

AWR (J6)                            ESP32

MCUCLK OUT (pin 5)         SCK (pin D8)

SPI_CS (pin 6)                    D0

SPI_MOSI (pin 12)              MOSI (pin D10)

SPI_MISO (pin 14)              MISO (pin D9)

What do I need to do to get this SPI communication working on the AWR1443 end? (The AWR1443BOOST board is running the default demo program).