Other Parts Discussed in Thread: ENERGIA, PGA460
Tool/software:
Hello TI,
We were initially using PGA450, but now we selected PGA460 for our distance measurement application. We are trying to interface PGA460 with Pi4 over UART. We have ported the Energia library to be compatible with Ubuntu OS.
We are getting response from PGA460, but it seems reception is incorrect. Also, distance is not changing and we are always getting constant value.
I have the following queries:
- I wanted to ask if there is any way to check the correctness of UART communication with PGA460 similar to Comman 0 which is used to test PGA450 UART communication.
- As we ordered PGA460 BOOSTXL Evm for initial evaluation, is it necessary to flash it before getting started?
- In our custom board, we will use PGA460, do we have to flash / update firmware before we can use it?
Would be waiting for the response.
Thanks & Best Regards,