This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: Problem when running awr2944_mmw_nonos TDM demo

Part Number: AWR2944

Tool/software:

Hi,

Customer reported that they can't make awr2944_mmw_nonos TDM demo working.

I imported the awr2944_mmw_nonos TDM demo from radar_toolbox_2_10_00_04\source\ti\examples\nonos_oob_2944. Rebuild and run. I met problem either.

1. The default cfg in sdk can't work. I need to remove the comment info with % and only leave the commands.

profile_2d_2AzimTx2.cfg

2. After I load the cfg in visualizer manually, I saw sensor start done, but no point cloud showed on GUI.

3. I connected CCS and found the DSS code is asserted. It seems the DSP processing can't finish in one frame. So I tried to increase the frame period to 800ms, but still failed. 

Would you pls help to check what's wrong and solve the problem?

Thanks,

Chris