This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: short range radar, angular resolution

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: AWR2243BOOST, AWR2243

Tool/software:

Hello,

I want to test radar for an application, where an angular resolution in the range of the MMWCASRF-EVM is needed. The application only has to detect targets up to a range of 10m. As the range of the design states a range of >350m the question arises if this is the suiting development kit for that application or if a dedicated short range radar development kit should be used. I did not find any short range kits with that angular resolution.

Thanks!