Other Parts Discussed in Thread: IWR6843AOP
Tool/software:
Hi,
The 3d people count project under the workspace of CCS, We would like to modify gtrack_create.c file of Gtrack.
But this gtrack_create.c file is located under c:\ti\mmwave_industrial_toolbox_4_12_1\labs\common\src\alg\gtrack\src.
How do I put the C file modified under Gtrack folder into the entire CCS project for compilation?
Should I drag Gtrack folder to 3D_people_count_68xx_mss in the project and then execute the build project? ( Is this the right way?)
After build project, can I include the binary file generated by the modified C file of Gtrack?
Environment:
mmwave_sdk_03_05_00_04
mmwave_industrial_toolbox_4_12_1
project: 3d_people_count_68xx ( with mss and dss)
IWR6843AOP
Thank you.