This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843: Pointcloud SNR value too high

Part Number: AWR6843

Tool/software:

Hi,TI engineers,

I'm using sample code : AWR6843_CPD_with_Classification and i have some question about calculation of SNR

as following figure,

and i saw that the snr/ noise 's scale was described 0.1 dB.

I converted the raw bytes into int16 and multiplied the value with 0.1,but i still got the too large value(some point more than 300), i think it is not reasonable.

I noticed that the noise term in the SNR calculation formula had been multiplied by 8. Does this 8 have any specific meaning?

Regards ,
Juncheng