Tool/software:
Hi,
I want to implement long-distance ranging (10m~100m) with the IWR1843 and achieve centimeter-level accuracy, prioritizing precision.
Q1:
Can I achieve this with the MRR code? I have also looked into the level_sensing demo. Can Zoom-FFT solve this problem?
Q2:
If I use the level_sensing demo, can I change the antenna configuration to three transmit and four receive (3T4R)?If so, what is the maximum measurement distance and accuracy that can be achieved?The current version of the level sensing demo is 1843. I tried modifying the CLI command to channelCfg 15 7 0 for the three transmit and four receive mode, but when connecting to the GUI, nothing was displayed.
I need technical support from TI.
Regards.
Henrry