Hi,
I conducted an experiment where a car drives towards the radar. The car starts accelerating at approximately 40 meters and reaches a maximum velocity of 47 km/h (13 m/s).
As shown in the screenshot below, the velocity measured at 25 meters is -21 m/s, which is twice the expected velocity and much higher than the true measured maximum, 13 m/s.
I'm using single Tx and 4 Rx.
Can you explain this discrepancy?
Thanks,
Shlomi