This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: load CFG on boot automatically

Part Number: IWR1843BOOST

Tool/software:

Im using IWRL1843boost for traffic monitoring,

how can I make the .cfg load on board boot automatically?

is the "Hard code config" applied to this board?

which .cfg is recoomand? I found there are 2 .cfg inside the radar_toolbox_2_10_00_04\source\ti\examples\Traffic_Monitoring\chirp_configs:

18xx_traffic_monitoring_70m_MIMO_2D.cfg and 18xx_traffic_monitoring_70m_MIMO_3D.cfg

  • Hello,

    You can use the same methodology used to add a hard coded config as seen in the fundamentals user guide. As for the two configuration files it depends on what you care about for the demo/application at hand. The 2D vs 3D configurations are as the file name say, one uses two antennas for 2D and one uses three antennas to get elevation for that 3rd dimension. People who do not care about the Z-axis/elevation of a scene can save power and processing time by only using the two dimensions they care about.

    Best Regards,

    Pedrhom