Other Parts Discussed in Thread: IWR6843
Tool/software:
Hello Community,
We are using IWR6843 HS chips on our custom boards. For development, we used IWR6843 QG (General/Non-secure) chips.
As far as I understand, High-Security devices are in Field securable (FS) mode and consist of TI keys when delivered from TI, and do not require a secure boot process.
So my questions are:
- Is it possible to directly debug this chip, without putting ccs_debug_secure.bin and using normal ccs_debug.bin inside to debug or connect with debugger at least when no image is inside?
- Can I transfer my unsecured IWR image directly into the chip, since it's still in FS(Field securable mode)?
- Can I use this chip just like the IWR6843 unsecured chip when in HS-FS mode?
Right now we just want to use this High Secure chip like normal General chip without putting any keys, is this possible with this chip?
If not how should I proceed to put an image or debug this chip?
Thanks and Regards,
Swapnil