This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOP: Inquery about interference management applied into Radar SDK

Part Number: IWRL6432AOP

Tool/software:

Hi L6432 and 6843 Champ !

My customer is looking at using the 6843AOP and L643AOP, a 60 GHz Radar, for a Setop Box solution.
They feel that the TV and Speaker Application Guide and Multi People Tracking Demo, featured in the Application directory of the Radar Toolbox, are a good fit for their use case and are actively considering the application.

One question during the sales promotion,

They are concerned about signal interference from other products with 24, 66, 77 GHz Radar installed in the same living space.
If there are multiple radar beams from different products within the FOV of the setop box with 6843AOP and L6432AOP, it is assumed that there will be interference problems.

Does TI have a solution to avoid interference or is it already reflected in the Radar SDK?

How can I distinguish between signals sent from my device and returned to me, and signals sent from other radar devices and only received by my device, so that I can filter them out or pick out only signals from my device?

Does the solution to eliminate such signal interference only work with DSPs? Can it be applied to ARM Only devices such as L6432? Please tell me if there is SDK support for the interference management solution and whether it can be applied to each device?

Please let us know about the availaibility of signal interference management solution and applicable device.

Thanks.

Best Regards, Jack Cha