This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2544: Hardware Trigger SYNC_IN

Part Number: AWR2544
Other Parts Discussed in Thread: AWR2243, AWR2243BOOST,

Tool/software:

I have an existing functional setup with multiple AWR2243 combined with DCA1000. I'm using the SYNC_IN Pin to trigger them simultaneously. I want to switch to the AWR2544. I saw that there is no Pin-Connector with the SYNC_IN signal anymore. I traced the signal path and found some possible positions with solder pads to apply a cable.

So is it possible to trigger them over the SYNC_IN signal? I tried but the DCA1000 did not record anything so i think the triggering over the SYNC_IN Pin did not work.

Best regards
Oliver