Other Parts Discussed in Thread: IWR6843, IWR6843ISK, IWR6843AOPEVM
Tool/software:
1) Our requirement is to deploy a robot that can clear snow from sidewalks. The snow can conceal various objects beneath it, such as fire hydrants, stones, or even animals ( dogs).
2) The robot moves at a slow speed of 20 mph, and we need it to have a clear view up to a range of 10 meters.
Key requirements:
- A 360-degree view with a range of 10 meters and high resolution to identify objects under the snow.
- Capability to detect both stationary and moving objects.
- Low power consumption, as the robot operates on a battery.
- Preferably with a CAN interface.
- An evaluation board with a USB port would be beneficial for initial testing on a Windows laptop.
Please guide us in figuring out what radar sensor evaluation boards we can use.