This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Custom based AWR1843 board

Part Number: AWR1843


Tool/software:

Hai....., In the given document " TImmWaveRadarsensorRFPCBDesign,Manufacturing andValidationGuide " it is given :- L1 to L2, ground, microvia 1) 150 um drill diameter 2)300 um via L1 pad diameter.

Since our fabricator supports 1:1 aspect ratio for microvia,

If possible could you simulate our via transtions(200um drill and 450um pad) , the material we are using is Ro3003 with thickness 5mil. 

Will there be any issue if we are going with our transtions.

Thank you.