This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: What format is the data that only has the real part transmitted

Part Number: AWR2243


Tool/software:

Hello,

I am using awr 2243 for the design, the current configuration used is 16-bit adc, the format of csi2 is raw8, transmitting chirp parameters + raw data. If csi2 is set to transfer complex data, the data can be received normally. If csi2 is set to transmit only real data, the received data is wrong.

So I would like to ask, if only the real part is transmitted through csi2, what is the format of the transmission?

The following figures correspond to the data format of the complex, raw8

Hope to receive a reply as soon as possible. Thank you