Tool/software:
Hi Team,
The customer is proceeding with the design with reference to Table 9-5.
They are considering using it with the following contents.
- Continuous conversion mode in VDD power supply mode, one conversion every 0.125 seconds (average of 8 consecutive conversions)
Is the following sequence correct?
1) Reset
2) SKIPADDR (device selection)
3) WRITE SCRATCHPAD-1 (register setting)
4) Idle time 1s
5) Reset
6) SKIPADDR (device selection)
7) READ SCRATCHPAD-1 (temperature result reading)
8) Reset after receiving the first 8 CRCs
9) Repeat 4) to 8) every 1 second.
Best Regards,