Other Parts Discussed in Thread: AWR2243, MMWCAS-DSP-EVM
Tool/software:
Hi,
I'm using the MMWCAS-RF-EVM along with the MMWCAS-DSP-EVM to collect data using mmWave Studio 3.0.0.14. The RF-EVM has AWR2243 radars and is connected to the computer with the required ethernet cable, usb cable, and 12V 5A power supply. I have used the scripts provided by mmWave studio for the cascaded radar and have used the Cascade_Configuration_TestSource.lua for configuration of devices and Cascade_Capture.lua for capturing data. The Cascade_Configuration_TestSource.lua works perfectly but when I run the Cascade_Capture.lua script i'm getting the error: create application response from capture card timed out!! TDA ARM failed error, as seen in the picture below. I have tried restarting the radar along with mmwave studio multiple times as well as restarting my computer but nothing seems to work. Is there anything i'm missing perhaps? Any help will be appreciated.