This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: PGA970EVM

Part Number: PGA970

Tool/software:

Hello,

I hope you are well,

Customer is claiming that part: PGA970EVM is defective:

Inconsistency of the signal generator frequency of the PGA970EVM: EVAL
BOARD FOR PGA970 branching tool with the parameters specified in the
settings.
When checking the signal parameters, it was determined that the DAC
sampling frequency of the debugger signal generator is 532 kHz, which does
not meet the specification (according to the MHz specification).

It looks that part is out of warranty (Above 90 days from invoice),

Could you please advise if we are able to support Customer to help him resolve that issue?

Thank you for the support,