This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: IWR1843BOOST Usage exception

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: UNIFLASH, IWR1843

Tool/software:

Hi

Problem 1: Step 2 RS232 in mmWave studio is not connected

Problem 1: Step 2 RS232 in mmWave studio is not connected
Question 2: Do I need to use uniflash to write demo to IWR1843 before using mmWave studio
Question 3: Where should s2 sop sw1 sw2 s1 in IWR1843 and DCA1000 go
Question 4: Does IWR1843 DE SOP ON represent 1 switch of DCA1000? Is sw1 ON the left side 12BIT_ON represents 1 switch of DCA1000? Is sw2 ON the left side ON represents 1 switch of DCA1000? What is the status of s1
Problem 5: The DCA1000 does not connect the memory card separately and uses the status of the data switch SW2 on the PC

Please help confirm the above questions, thank you