This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC5072-Q1: Can't startup. Goes to bootloop

Part Number: LDC5072-Q1


Tool/software:

I'm trying to start a PCB sensor that was running on an IPS2550 (from Renesas) but it can't initialize.

It's trying to start every ~29 ms during 4 ms and that's all.

Sensor characteristic: Lexc = 1.1 uH, Rexc = 2.4 Ohm, Clc = 2 nF (NP0). Resonant frequency on IPS2550 is about 4.9 MHz.

Lin = 900 nH, Rin = 2 Ohm. Gain about 20.

How can I track the issue?