This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: which software to use for raw data capture?

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243

Tool/software:

Hello,
Currently I am working with AWR2243BOOST connected to a DCA1000 for raw data acquisition.
For hardware setup first i need to check:
1. switches
2. jumpers
3. power 5v for both or just DCA1000?(as  i have connected both with 60 pin interface)
or will DCA1000 can power up AWR2243 by just a switch?
4. ethernet and usb connections to pc.

After Hardware setup
The software i need to install are:

  • Code Composer Studio (CCS)
  • mmWave SDK
  • XDS Emulation Software Package (if necessary)
  • mmWave Studio
  • MATLAB Runtime Engine v8.5.1

    Are all these software required for raw data acquisition?

    And one more doubt mmWave Studio or MMWAVE-STUDIO-2G.

    How to setup these software after installing?