Other Parts Discussed in Thread: AWRL6432BOOST
Tool/software:
Hello expert,
I successfully executed mmWave example binary demo from Flash and checked the behavior with Visualizer.
As a next step, we would like to run it from the example code.
(Is the binary code compiled from the example code?)
MMWAVE_L_SDK_05_04_00_01\examples\mMW_demo\mmwave_demo\xwrL64xx-EFM\m4fs0-0_freertos\TI-arm-clang
Imported from CCS, compiled, and debugged (emulated) from CCS.
When I started debugging in the default state, an error occurred.
Debug -> Connection Options -> Reset the target on a connect check.
Verified that the following is displayed when the tera term is connected.
*************************************
XWRL6432 MMW Demo 05.04.00.01
*************************************
Then, when I entered the CLI command and sensorStart, I received the following error:
(Use the command by copying the output from the Visualizer Window in the default example binary mode.)
Do I need to change the config settings?
Error: FECSS RF Power on/off failed
Error: MmWave Control Initialization failed [Error code -203227134] [errorLevel 2] [mmWaveErrorCode -3101] [subsysErrorCode 0]
Exception: ../factory_cal.c, line 338.
[Environment]
AWRL6432BOOST
CCS12.7.1.00001_win64
Xdsdfu firmware_3.0.0.29.bin
MMWAVE_L_SDK_05_04_00_01
Could you please help to solve this issue?
Regards,
A.Fujinaka