This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA460: Operation at 125KHz

Part Number: PGA460
Other Parts Discussed in Thread: TUSS4470, TUSS4440

Tool/software:

Is there a version of the PGA460 that can generate a 125KHZ drive signal for the transducer?  

  • Hello Robert,

    Thanks for posting to the sensors forum! Unfortunately we do not  have a version of PGA460 that can drive a transducer at 125kHz. We do have other devices like TUSS4470 or TUSS4440 that are capable of this but are different from the PGA460. The PGA460 does operate from 30-80kHz and 180-480kHz so if you are able to use a transducer in one of those frequencies then the PGA460 is a suitable solution.

    I hope this helps!

    Best,

    Isaac