Tool/software:
When running the attached lua file on mmwave_studio_04_01_00_06, there was distortion in the waveform of the IF signal.
The setting is configured to transmit two chirps within one burst.
It does not occur in Chirp 1, but it occurs in Chirp 2.
Please tell me the cause and countermeasures.
Chp1
Chp2