Other Parts Discussed in Thread: TSD05, TMAG5110
Tool/software:
Hello E2E Community,
We are planning to use the TMAG5111 2D Hall Effect latch for our next project, which requires separate outputs for speed and direction sensing.
I have a specific query regarding the detection of direction after a system reset. Here's the scenario:
- The machine starts from zero, and we allow an initial stabilization time of 1 second.
- The sensors record rotational speed and direction.
- The system is then switched off and restarted in the reverse direction.
In this case, while the speed detection is straightforward, I want to confirm the behavior of the direction output. Specifically:
- For clockwise rotation, will the direction output consistently be high?
- For counter-clockwise rotation, will the direction output consistently be low?
Is it correct to assume that, regardless of the system's configuration and state, we can map the direction output as high for one direction and low for the other?
Also, do we need to install ESD diode close to the sensor? We plan to minimize the component count near the sensor by using only decoupling MLCC of 0,1uF - let us know if we can simply add 27Ohm pulse proof resistors on OUT1 & OUT2 pins for some safety while having a TVS diode installed on the MCU side (TSD05)? Or do we also need to install the TVS diodes near the Sensors? Our system works on 5V DC & the length of the wires shall be no more than 3m from the host MCU.
Your insights would be greatly appreciated.