This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: OPT3101 laser pulse period

Part Number: OPT3101


Tool/software:

I have a question about the OPT3101 laser pulse period.

OPT3101 always acquires data at 4000Hz and determines the sampling rate with NUM_SUB_FRAMES.

In other words, 4000 pieces of data are divided by NUM_SUB_FRAMES, averaged, and the measurement is calculated.

This is written in the data sheet "7.3.1.3 Non-HDR Mode".

So, I'm curious about the laser pulse during measurement. Can you tell me the number of times the laser pulse lights up per second and the lighting period?