This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2010: HDC product recommendation

Part Number: HDC2010

Tool/software:

Hi team,

do we have recommendation for below request? better to be latest roadmap product with better cost.

Working voltage: 3V
Working temperature and humidity range: -40~125℃, 0-100%RH
Temperature and humidity test accuracy: ±0.3℃, ±3%RH
Power consumption requirements: average current <1uA, standby current <100nA
Package: conventional SMD package
Data transmission: support I2C
Test response time: <10ms
ESD requirement: 2KV
Optional function: built-in heating function