Tool/software:
We are planning to use the HDC3022 temperature and humidity sensor in a low pressure environment.
If this sensor is calibrated using the provided calibration tables in an environment of 1013mb, how accurate will the humidity sensor be in a low pressure environment? Is a recalibration required if the sensor is moved to a low pressure environment, and if so, can the provided calibration tables be used?
We do not require high accuracy of humidity data for our application, an accuracy of ~2% would be sufficient.