This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: The power indicator light on the DCA1000EVM is abnormal

Part Number: DCA1000EVM


Tool/software:

I recently purchased a DCA1000EVM to study radar-related knowledge, but I encountered an issue during initial use. I'd like to ask if the following situation is normal:

When I connect the power using a 5V/2.5A adapter(I have confirmed in advance that this power supply can properly power the AWR1642-BOOST), should the power indicator on the DCA1000EVM remain constantly on or flash? Mine does not remain constantly on. Is this indicative of a hardware malfunction? If so, can I request after-sales support?