Other Parts Discussed in Thread: TMP235, ISOTMP35
Tool/software:
Dear Friend
My application is to protect a linear Mosfet from overheating with possible heavy/overstressed usage. the Mosfet is surface mounted with its drain connected to a piece of copper on top of PCB. My plan is to mount the TMP236A2DCKR near the Mosfet with its body glued on the same piece of copper by Kafuter K-5204K Silicone Adhesive Paste. My questions are:
1. Is my plan good enough for the sensor to sense the true case temperature of the Mosfet?
2. Should/Can I connect pin1 and pin5 of the TMP236 to the same piece of copper?
3. Any other better thermal design in such applications?
Best Regards
Tony