Tool/software:
Hi ti team,
1. It is impossible to operate the register. Even if writing is repeated multiple times, the value read from the register is still always a default value (attempts have been made for the two registers 0A and 0B). Even after replacing the photosensitive board, the problem persists. Through the inspection with a logic analyzer, the written device address, sensor address and the value are all accurate. 2. Is it necessary to initialize when operating the register? If so, can you provide the example code (demo code)? 3. Does the brightness value and the xy value belong to one of the four channels or the combined data of the four channels?