Other Parts Discussed in Thread: TX12
Tool/software:
Hello,
I am currently using MMWCAS-RF-EVM+MMWCAS-DSP-EVM.
I have three questions.
1. Are the device numbers in the figure below correct?
Device No.1: Master, Device No.2: Slave1, Device No.3: Slave2, Device No.4: Slave3
2. Are the TX numbers in the figure below correct?
TX1: Tx2 of Device No. 1, TX2: Tx1 of Device No. 1, TX3: Tx0 of Device No. 1,
TX4: Tx2 of Device No. 2, TX5: Tx1 of Device No. 2, TX6: Tx0 of Device No. 2,
TX7: Tx2 of Device No. 3, TX8: Tx1 of Device No. 3, TX9: Tx0 of Device No. 3,
TX10: Tx2 of Device No. 4, TX11: Tx1 of Device No. 4, TX12: Tx0 of Device No. 4
3. Are the RX numbers in the figure below correct?
RX1: Rx0 of Device No. 1, RX2: Rx1 of Device No. 1, RX3: Rx2 of Device No. 1, RX4: Rx3 of Device No. 1,
RX5: Rx0 of Device No. 2, RX6: Rx1 of Device No. 2, RX7: Rx2 of Device No. 2, RX8: Rx3 of Device No. 2,
RX9: Rx0 of Device No. 3, RX10: Rx1 of Device No. 3, RX11: Rx2 of Device No. 3, RX12: Rx3 of Device No. 3,
RX13: Rx0 of Device No. 4, RX14: Rx1 of Device No. 4, RX15: Rx2 of Device No. 4, RX16: Rx3 of Device No. 4
Regards,
Tsuda