Other Parts Discussed in Thread: AWR6843
Tool/software:
Dear sir:
We saw in the LRPD documentation for the 6843AOP that the 6843AOP can achieve a chirp configuration containing three TXs in the same frame, as shown in the image below.
If we want to achieve the same effect in CPD, how should we modify the configuration file, or do we need to flash additional firmware?
Here is the configuration file we are currently using:
Additionally, I would like to ask about the idleTime
parameter in the profileCfg
section of the configuration file. Why is one set to 2789 while the other is set to 20?
Best regards
Hsiu-Che Chang