This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOP: How to release the static point cloud in 6843AOP?

Part Number: AWR6843AOP


Tool/software:

Hi,

Here are the more details of the question.

In CDP demo,I need to observe the static point clouds.But now when there is no moving target in the test sense,no point cloud can be seen.

How to config some parameters such as Static or dynamic CFAR parameters to implement it?

Looking forward to your reply. 

  • Hello,

    If you would like to pick up static objects, you will need to disable clutter removal which subtracts the mean values of the input samples to the 2D-FFT to mitigate static objects. This can be done by using the following CLI command and parameters: clutterRemoval -1 0.

    Regards,

    Kristien