Tool/software:
Hi,
Is it possible to update the config file or firmware of radar IWR6843 over the air? If yes, then is there any project in labs is available which I can refer to?
Thanks,
Manoj
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
Is it possible to update the config file or firmware of radar IWR6843 over the air? If yes, then is there any project in labs is available which I can refer to?
Thanks,
Manoj
Hello Manoj.
The SBL will allow over-the-air updates by allowing the user to send the binary via UART even when the device is in functional mode. Please refer to the SBL example in the SDK for more information.
Sincerely,
Santosh