This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-C2000EVM: TOF doesn't change even when I change the position of the Transducer.

Part Number: TDC1000-C2000EVM

Tool/software:

I have the above configurations and I am trying to find the TOF that I can feed into the formula, D=(TOF X speed of sound)/2 to get the length of the container but even when I change the position of the transducer, the TOF does not change. It remains constant even when the transducer is not attached to the container. What could be the problem?

The container is filled with water at room temperature.