This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Get data from IWR1642BOOST

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Tool/software:

Hi,

I have designed an interface board that I want to use to communicate with the IWR1642 BOOST radar via the network. Currently, I can send config through the network to RS232 and receive "done," but I am not receiving anything from the MSS logger. After receiving the "done" message from the last sensorStart command, should the MSS logger produce any output ?Do I have to do something else after sending config so that I can get the output?

I have set the baud rate to 921600.