Tool/software:
An issue of "Power Disabled upon power up" came up, based on what the default ALERT output is at power up. Is ALERT = HiZ on power up, before it gets programmed.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jack,
The alert pin of TMP110 features an open-drain interface. By default, the alert pin is configured to be active LOW. Thus, on POR, alert will be at HiZ state--assuming that the end-user is implementing a pullup resistor, the voltage on the line will be read as a logic high. It is also important to note that if the junction temperature is higher than 80°C on POR, the device will pull the line down after the first temperature conversion since this temperature is above the POR value of the high alert limit.
Best regards,
Simon Rojas