This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC3020: Please help to check if there are any issues with the schematic diagram

Part Number: HDC3020


Tool/software:

Please help to check if there are any issues with the schematic diagram. If there are any problems, please provide detailed explanations and suggestions for modification. Thank you!

  • Tony,

    You don't need 10Kohm resistors to connect the ADDR and ADDR1 pins to VDD or GND, 0ohm jumper resistors would be better. Are there pull up resistors elsewhere for SDA and SCL? At a minimum a pull-up resistor is needed for SDA.

    Regards

    -Alex Thompson