This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMCS1123: TMCS1107

Part Number: TMCS1123
Other Parts Discussed in Thread: TMCS1107EVM

Tool/software:

What is the best hall-effect current sensor for measuring DC current, ranging from 1A to 85A with Vs=3.3V.  Thank you

  • Hello,

    The TMCS1123C1A is the closest part to your requirements. However, the TMCS1123C1A cannot measure 85A at a 25°C ambient temperature because it will exceed the SOA (safe operating area) mentioned in the Datasheet:

    If you can keep the RMS current below 80A you should be able to use this part for your application.

    This curve assumes that you are using a layout similar to the TMCS1123 EVM linked here: https://www.ti.com/product/TMCS1123. It is also possible that you could improve the thermal performance of the TMCS1123 EVM with a better layout, or implementing active cooling.

    Let me know if you have any more questions,

    Levi DeVries

  • Hi Levi,

    Thanks for your answer.

    I am about to layout a PCB for TMCS1107A2U using Altium.  I wonder if I can have the design package of the EVALUATION BOARD (TMCS1107EVM).

    For this application, I just need to measure current from 0 Amp to 25 Amp.  Can I design with only 1 oz. of copper thickness?

    Please advise.

    Thanks

  • Hello,

    The thickness for the EVM is 3oz of copper thickness on two outer layers, so I am doubtful that only 1oz of copper thickness will provide enough heat dissipation for 25A.

    I have sent you a friend request to send you a copy of the TMCS1107EVM design.

    Thanks,

    Levi DeVries

  • I got the TMCS1107EVM design. Thanks for your helps